Post Go back to editing

AD7829

8通道模数转换芯片AD7829外围电路和时序都正常,但是有时加电后不能工作,即给了/CONV转换启动信号后,芯片没有转换结束信号/EOC输出。但是重新断电加电后,芯片工作又正常了,求帮助!!

  • 1. VDD上电后多长时间,开始发/CONV脉冲开始转换的?AD7829 have a 1 μs power-up time when using an external reference and a 25 μs power-up time when using the on-chip reference.

    2. 可以尝试用一个4.7kohm电阻,把/CONV上拉到VDD试试。

  • 感谢您的回复!

    我在一个项目中分3个区域共计使用了135AD7829,每个区域用1FPGAAD7829进行操作。加电后首次工作的时间是在几十秒或是几分钟以后。我们/CONV信号线开始是悬浮的,出现问题以后,我们将部分/CONV信号线进行了下拉处理,问题没有得到改善。感觉AD7829不能工作是在加电瞬间决定的,所以我们对加电过程进行了处理,即由原来的3个区域同时加电改成3个区域分别加电,进行此项改进之后,AD7829不能工作的情况得到改善,但还是没有完全得到解决。现在的完全解决方法就是当有某个区域的AD7829不能工作时,将此区域进行重新加电处理,一般重新加电两到三次,AD7829将会全部工作。

        还有一个疑惑:有部分的AD7829我是用一片电源转换芯片给2AD7829供电的,这2AD7829会出现1片工作正常,1片不能工作,也就是说这两片AD7829工作环境应该是基本一样的,但结果却不同,百思不解。