Post Go back to editing

变送器AD5412/22/10/20常见问题解答

ADI中国技术支持团队精心整理了有关变送器AD5412/22/10/20的常见问题解答文档。想了解ADI专家们是如何解答以下常见问题吗?赶快下载文档吧!

 

问题1 AD5420PIN 1451211均为GND,数字地和模拟地应该怎么区分?

问题2 AD5420的评估板中的R27电阻的作用?

问题3 AD5422EPAD脚如何处理,与什么连接呢

问题4:在使用AD5422的过程中,选择0-5V输出范围,code=0000时,输出为0.027Vcode=FFFF时,输出为5.89V

问题5 AD5422的数据手册上显示使用外接Rset电阻精度会更高,那么Rset的精度和温漂应该如何选取;同样的使用外接的referernce也能提高精度,那么reference如何选取

问题6 AD5422的内部Rset电阻的温漂是多少

问题7:是否有AD5410/20/12/22的示例代码

问题8 AD5420输出接1KΩ的负载,code=0000输出为3.98mA code=7fff输出为11.92mAcode=FFFF输出为14.07mA,为何FFFF时不正确?

问题9:是否有针对AD5410/20/12/224-20mA变送器完整的隔离方案?

问题10 AD5410/20/12/22都是单通道输出的芯片,是否有多通道的芯片?

问题11 AD5410/20/12/22AD420的区别?

 

如果您还有关于变送器AD5412/22/10/20的疑难问题,请在这儿(http://ezchina.analog.com/post!input.jspa?container=2003&containerType=14)告诉我们吧



attachment.pdf
Parents Reply Children
No Data