Article 环路供电变送器AD421/AD5421常见问题解答

Loop Powered Transmitter AD421/AD5421 FAQ by adiadmin

The ADI China Technical Support team has carefully compiled the FAQ documentation for the transmitter AD5412/22/10/20 . Want to know how ADI experts answer the following frequently asked questions? Download the document now!

 

Question 1 : Is the circuit of the current loop necessary to be separated from the AD421 or AD5421 ?

Question 2 : The FET tubes provided in the data sheet are difficult to buy. Is there any other alternative ?

Question 3 : How can I control the programming of the AD421 and AD5421 through a microcontroller ?

Question 4 : Why does the current output of the AD421 not match the value I programmed?

Question 5 : If I want the AD421 to supply more than 20mA , can it?

Question 6 : When the AD421 or AD5421 supplies power to other devices, why does the loop current become inaccurate?

Question 7 : How to build a current source with the AD421 ?

Question 8 : How should the FET pin be connected to the AD421 ?

Question 9 : Why is the DN2540 vulnerable to damage?

Question 10 : The current on the current loop, at 7-20 mA , the measured data is basically the same as the set value. However , the error is very large below 7 mA , and the actual measurement is 6.5 mA at the output of 5 mA . why?

Question 11 : Can I use one power supply to provide loop power to two AD421s ?

问题12:采用下面的电路图,这里光耦型号为4N28,发现当上拉电阻为4.7k 时输出电流不正确,而当上拉电阻为10k时,输出电流正确。为什么?

问题13:AD421 评估板原理图中,28F0195-100 是用于EMI 抑制的,是否有其他替代器件推荐?

问题14:ADI公司还推出可以替代AD421或者与其类似的产品么?

问题15:AD421与AD5421的区别?

问题16:如果环路供电的系统中,外围器件的功耗需求会大于3.25mA/3.15mA,是否有什么方法来解决二者之间矛盾?

问题17:如何确定环路供电的传输电缆长度?

问题18:为何芯片有时发热比较厉害,芯片功耗与芯片的工作电压、电流以及温度间有什么关系?

问题19:使用万用表测量电流值正确,而使用示波器时测量的电流值不准确?

问题20:AD5421无CS引脚,是否可以使用SYNC当做CS管脚使用?

如果您还有关于变送器AD5412/22/10/20的疑难问题,请在这儿

(http://ezchina.analog.com/post!input.jspa?container=2003&containerType=14)告诉我们吧!

 

5670.attachment.pdf

RE: 环路供电变送器AD421/AD5421常见问题解答 by adiadmin:

产品简介

 

AD421是ADI公司推出的一种单片高性能数模转换器(DAC) 。它由电流环路供电,16位数字信号串行输入,4~20 mA电流输出,完全符合设计智能变送器的工业控制标准信号输出要求,可实现远程智能工业控制。它内部含有电压调整器,可提供+5V,+3.3V或+3V输出电压,可为其自身或其他电路使用。AD421采用ΣΔDAC结构,保证16位的分辨率和单调性,其积分线性误差为±0.001%,增益误差为±0.2%。AD421支持HART通信协议。标准三线串行接口可在10 Mbit/s下运行,便于与微处理器或微控制器相连。

AD5421是AD421的升级版本,也是一款完整的环路供电型4 mA-20 mA数模转换器(DAC),专为满足工业控制领域智能变送器制造商的需求而设计。相比AD421,其拥有更好的精度、温度范围以及工作电压范围。AD5421内置一路稳压输出,用于为自身及变送器中的其它器件供电。此调节器提供1.8 V至12 V的调节输出电压。该器件还内置1.22 V和2.5 V基准电压源,因而不需要分立调节器和基准电压源。AD5421可以结合标准HART® FSK协议通信电路使用,而且额定性能不会受到影响。高速串行接口能够以30 MHz速率工作,并且允许通过一个SPI兼容型三线式接口与常用的微处理器和微控制器简单相连。AD5421保证16-bit单调性。典型条件下,积分非线性为0.0015%,失调误差为0.0012%,增益误差为0.0006%。

AD421

产品详情、技术参考文档、参考设计、样片申请及购买:

https://www.analog.com/en/digital-to-analog-converters/da-converters/ad421/products/product.html

Search related forums for AD421 :

Http://ezchina.analog.com/search.jspa?q=ad421

AD5421

Product details, technical reference documents, reference designs, sample applications and purchases:

https://www.analog.com/en/digital-to-analog-converters/da-converters/ad5421/products/product.html

Search related forums for AD5421 :

Http://ezchina.analog.com/search.jspa?q=ad5421

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.