MAX5113GTJ+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX5x
MAX5113GTJ+: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX5113如何通过SPI设置电流输出?
MAX5113的SPI通讯数据格式采用地址+R/W+数据的格式。地址+R/W(命令字节)为8位,数据为16位,因此,一个SPI通讯需要发送24个时钟周期。需要注意的是数据手册给出的地址为R6-R0,在发送时由于最后一位为R/W,所以需要将数据手册给定的地址左移一位,比如对地址0x04寄存器写数据时,需要发送0x08+R/W 位。当命令字节和数据发送完成后,要将/CS拉高。 根据应用需求配置各通道寄存器以及通用配置寄存器…
MAX5113当输入的码字在某个数值m(m大概在100左右)以下时,DAC各个通道的输出均为0,是什么原因?
参考数据手册如下,MAX5113的各个输出通道都预设了负的offset,使得输出能到0.
MAX5113的输出毛刺指的是什么,对电路设计有什么影响
由于DAC的内部工作原理,当DAC的输出发生变化时,会产生一定的过冲。这个现象定义为输出毛刺(DAC Glitch impulse )。以MAX5113为例,它的输出毛刺指标在数据手册的第四页给出。 1)一般情况下,输出毛刺的大小与跳变的大小相关。数据手册里给出的指标是glitch impulse @ Major-Carry Transition。关于Major-Carry Transition的定义…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.