MAX1619: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX1619: FAQ
MAX1619
Sensors and MEMS
Temperature Sensor and Control Devices
Created
over 8 years ago
Updated
3 months ago
Was this helpful?
Yes
No
More
Cancel
MAX1619是每4秒读一次remote温度测量,这个频率是否可以配置,比如一秒读一次,或者两秒读一次?
这个是可以设置的,上电默认是4秒一次,可以通过寄存器配置,见下表:
MAX1619测量FPGA温度,当FPGA运行某些程序时,cpld读取的max1619的local和remote值,跳动很大,应该是完全异常的情况,这可能是什么原因?
如果Local和Remote的温度都发生跳变的话,建议检查一下电源,看是不是电源上的噪声比较大。对于模拟信号的测量,通常外部干扰会造成测量结果跳动。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.