MAX16141AAF/V+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX16141AAF/V+: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX16141在休眠模式下是否保持过压保护功能?
MAX16141在休眠模式下,MOSFET栅极控制电路是关闭的,器件仅消耗10µA电流,但可以通过体二极管向负载提供400µA电流(如下图中绿线所示),以保持某些关键电路的供电。
如何理解MAX16141的理想二极管特性?
MAX16141故障保护电路兼具了理想二极管控制器功能,原因是其内部集成了一个快速响应比较器,当输入电压跌落到输出电压以下某个设定门限(如下图所示)时,MAX16141将在 1µs (max)内控制外部MOSFET断开。由于MOSFET与外部二极管相比,压差非常小,故称其为理想二极管特性。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.