MAX1470EUI+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX1470EUI+: FAQ
Created
over 8 years ago
Was this helpful?
Yes
No
More
Cancel
”ESR最大不超过70 Ω”对MAX1470晶振有多重要?我需要在短时间内得到测试结果,而我找到的信号源的ESR不小于150 Ω,这样能工作吗?
控制环路设计用于承受较高的ESR。高ESR会增加电流消耗(稍微地)和“冷”启动时间(MAX1470不存在这个问题,因为它的振荡电路即使在关闭模式下也保持工作)。根据上述内容,较低的ESR更合适。
MAX1470 不同频率下的LNA输入阻抗是多少?数据手册列出315MHz下为50-j200。
MAX1470 LNA输入可以用一个50Ω电阻与一个2.5pF电容串联的模型表示。因此,433MHz下s11的值为50-j145。
在没有Rx信号时,MAX1470数据限幅器将比较噪声并产生伪信号输出。如何抑制这一噪声?
这是一种正常现象,可以通过在引脚20增加一个上拉电阻给限幅器加入一个滞回,但这将降低灵敏度。另一种解决办法是在发射端给信号加上同步头,使接收机能够区分信号和噪声。微处理器可以周期性地检测接收机输出,判断是否为有效信号。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.