MAX13488: FAQ

  • Created
Was this helpful?
  • MAX13488数据手册中的“input hysteresis”指的是什么?

    接收器高电平、低电平检测门限分别为+200mV和-200mV;25mV是叠加在接收器检测门限上的滞回电压。即RO输出高电平时,低电平检测门限将调整到-225mV;RO输出低电平时,高电平检测门限将调整的+225mV。
  • MAX13488的disable threshold是什么?

    DI为高电平时,MAX13488会关闭发送器。该门限电压是驱动器关闭之前必须检测到的A/B总线差分电压,只有检测到电压超出该门限后,驱动器才会关断。
  • RS485收发器在发送或接收数据时,允许总线引脚A,B上的共模电压范围是-7V至+12V?

    RS485规定总线共模电压范围为-7V至12V;Maxim大多数RS485收发器(比如MAX13488)的 A/B总线的共模范围可以达到-8V to +13V,甚至更高,优于标准要求。 由于共模电压范围是有限的,在构建网络时,对于非隔离架构,需要注意各个节点的地线连接,以避免地电位差在A/B线上引入过高的共模导致器件不工作,甚至失效。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.