MAX1230: FAQ

  • Created
  • Updated
Was this helpful?
  • 如果在MAX1230没上电之前对AIN输入电压是否会造成器件损坏?

    AIN 输入引脚电压范围是 -0.3V to VDD+0.3V. 因此,如果在上电之前对AIN施加电压,该电压会导致内部保护二极管导通,此时会从输入信号吸收电流,如果输入信号可以提供的电流小于50mA,则不会导致器件损坏,如果信号提供的电流大于50mA,则会造成器件损坏,因此,为确保器件正确工作,在器件上电后再对输入施加信号。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.