MAX11644: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX11644: FAQ
Analog to Digital Converters (ADCs)
MAX11644
Created
over 7 years ago
Updated
2 months ago
Was this helpful?
Yes
No
More
Cancel
MAX11644是一款I2C接口的ADC,但是和通常的I2C操作不一样,如何启动转换以及读取转换结果?
对于MAX11644内部的寄存器配置和通常的IIC通讯指定寄存器地址进行配置不一样,由于该器件只有两个寄存器,因此利用了寄存器中的最高位来指定寄存器地址,可以参考数据手册中的Figure9,当发送完从机地址并且让读写位为0,然后根据setup 和 configuration寄存器的数据格式发送数据就可以了。 启动ADC转换是利用读命令来启动的,ADC转换可以利用内部时钟模式和外部时钟模式,可以参考数据手册Figure10和Figure11…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.