MAX11410ATI+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX11410ATI+: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX11410 SPI通讯正确,设置PD = 00(normal mode),CTRL=0x63(internal, unipolar i/p, binary offset, Pside,N-side buffer bypassed, Ref Vdd/Gnd),MUX_CTRL0 = 0xAA ;PGA(0x0E) = 0x10 ;MUX_CTRL2 = 0x00;启动转换后,读取状态寄存器总是为0,是不是没有启动转换?
在对MAX11410初始化时,最好先进行校准操作,可以消除误差,除了配置上述寄存器外,还要配置Filter寄存器来设置转换速率,然后再启动转换,判断状态寄存器中的状态位--CONV_RDY,如果该位置1,则读取转换结果。 需要注意的是该位为读取清除,如果读取状态寄存器后,第二次再读取就会清除该位,因此可能造成读取全为0,常用的做法是设置中断状态,利用中断引脚来触发中断,在中断处理中去读取状态寄存器…
MAX11410测温精度问题
问题描述: 以前利用MAX11410来实现两通道测量,采用AIN0作为恒流源, AIN1和AIN2作为测量通道,实际应用中测量的温度精度符合要求,在新设计中需要实现4通道的测温,为节约通道采用了AIN0既作为恒流源,有作为测量输入通道,发现测温误差很大,请问这样设计是否有问题? ------------------------------------------------------…
利用控制器来读写MAX11410时,LED连接到MAX1410 GPIO,可以通过写寄存器来控制LED,但是读取任何寄存器时的返回值都是0xFF,如何解决?
对于MAX11410读寄存器操作,需要将读取的寄存器地址或上0x80,比如需要读取0x11寄存器的内容,发送的地址应该是0x80|0x11=0x91,因为最高位来决定操作是读还是写,当最高位为1时,表明时读取操作。
如果按照MAXREFDES1155设计两路RTD测温,是否还需要温度传感器MAX31723?
MAXREFDES1155参考设计中的温度传感器MAX31723用于热电偶冷端温度补偿,MAXREFDES1155本身可以支持RTD和热电偶温度测量,如果只是设计为两路RTD测温,可以不用使用温度传感器MAX31723。如果用于热电偶测温,则需要温度传感器。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.