MAX11300内部基准性能如何?
文档
Forums
Members
Tags
Cancel
Was this helpful?
Was this helpful?
Yes
No
In this Article
Created
over 8 years ago
Updated
7 months ago
文档
MAX1x
MAX11300: FAQ
MAX11300内部基准性能如何?
MAX11300内部电压基准的温度系数为±25ppm/°C;对于高精度应用,可以使用MAX6070等外部基准,温度系数为±6ppm/°C,甚至更高性能。
000098974
MAX11300
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.