MAX11214EUG+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX11214EUG+: FAQ
Created
over 8 years ago
Was this helpful?
Yes
No
More
Cancel
MAX11214单电源供电,输入毫伏级信号,PGA输出倍数不对,什么原因?
参考以下表格,MAX11214在PGA模式下,对输入电压要求必须大于VAVSS+0.3V, 输入毫伏级信号时请用双电源供电。
MAX11214在使用外部CLK的时候,频率范围是多少?
MAX11214的时钟CLK,其标称频率为4.096MHz。实际使用时,最高可用4.096MHz,最低可用1.024MHz。
MAX11214数据手册中的CMIRNG参数指的是什么?
CMIRNG指的是Common Mode Input Range, 即共模电压输入范围,在MAX11214的数据参数表中指的是Absolute Input Voltage. 如下表:
MAX11214输入超过负的基准电压,输出为全0,当输入为0时,输出也是全0,系统中如何区分这两种情况?
MAX11214状态寄存器中的bit2(DOR)可以用来指示转换结果是否超过了量程(超过了正基准电压或者负基准电压),如果该位为1,且转换结果为0,表示输入电压超过了负基准电压,系统可以通过该位和转换结果来判断输入电压的状态。
请问 MAX11214 在双电源供电时,参考电压需要双电源基准吗?
参考源不需要双电源,比如:+/-1.8V供电时,参考电压源范围介于0V与1.8V之间。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.