MAX11201: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX11201: FAQ
Analog to Digital Converters (ADCs)
MAX11201
Created
over 8 years ago
Updated
2 months ago
Was this helpful?
Yes
No
More
Cancel
MAX11201是否可以采用1.2V基准电压?
可以, Maxim在测试时使用了1.25V至VDD的基准电压,当基准电压超过该范围,器件仍可以正常工作。为确保可靠工作,建议选择符合数据手册要求的基准电压。
在MAX1201数据手册中对于模拟输入电压的限制是VGND+100mV 到VAVDD-100mV?但是按照数据手册图6的接法,模拟量输入电压范围是VGND,是否有问题?
MAX11201内部带有输入缓冲器,因此要求输入电压限制在VGND+100mV 到VAVDD-100mV,图6中将AINN和GND连接在一起是不正确的,这样会引起较大的测量误差,建议在AINN和GND之间连接一个电阻来”抬高“AINN的输入电压,使输入电压满足VGND+100mV的要求。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.