现在我在使用三片AD9914进行SYNC_CLK的同步,我现在使用AD9513已经实现了三片SYNC_IN的同频同相,同时对三片芯片做了统一的DAC校准和IO_UPDATE,但是我没办法利用SYNCLK,因为他的驱动能力太弱了,现在的情况是我现在所做的步骤无法使我三片DDS的SYNC_CLK同步,请问可能是什么原因呢?如果我不拿SYNC_CLK做参考这个同步是可能的吗?
REF_CLK是ADF4377提供的2.8GHZ提供给三片AD9914。
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Missed after 119 hours |
YANAMIANNA |
Closed |
现在我在使用三片AD9914进行SYNC_CLK的同步,我现在使用AD9513已经实现了三片SYNC_IN的同频同相,同时对三片芯片做了统一的DAC校准和IO_UPDATE,但是我没办法利用SYNCLK,因为他的驱动能力太弱了,现在的情况是我现在所做的步骤无法使我三片DDS的SYNC_CLK同步,请问可能是什么原因呢?如果我不拿SYNC_CLK做参考这个同步是可能的吗?
REF_CLK是ADF4377提供的2.8GHZ提供给三片AD9914。
我在论坛中看到了其他帖子有说AD9914的主频在2.5GHZ以上没办法实现多片同步是吗,我知道SYNC_CLK没办法自然对齐,所以我现在已经实现了SYNC_IN的对齐和REF_CLK的对齐,同时也做了统一的DAC校准和IO_UPDATE,但是还是没办法对齐,不知道是不是因为主频在2.5GHZ导致的,我看到有帖子说了