Post Go back to editing

ad9528 spi not respone

Thread Summary

The user encountered issues with the AD9528 not responding to SPI commands when used to generate JESD204B clocks for the ADRV9009. The problem was resolved by replacing the crystal, which was not providing a valid CMOS or LVDS signal. The AD9528 requires a proper CMOS or LVDS input for SPI communication to function correctly.
AI Generated Content
Category: Hardware
Product Number: AD9528
I have design a pcb use ad9528 to generate jesd204b clock for adrv9009. the schemtic is basiclly same as zcu102 and  adrv9009 eval board.
I try NO-OS sample of ADRV9009 .It exited at  read device id .
I have check the spi signal sended by xczu15eg, the waveform look ok.but ad9528 not respone .
can ad9528 spi with no crystal??
because I found my crstal is weied.
the out signal looks like a lvds with 1.5v common voltage 
the out_n is not a lvds signal with 0 common voltage 
I notice ad9528 crystal need cmos or lvds input 
I think this crystal is not a valid cmos or  lvds signal...
so: can ad9528 spi respone with no crystal???

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.