Post Go back to editing

AD9548 的参考输入REFA 单端输入的功率大小?8dBm 的10MHZ 信号可以吗

Thread Summary

The user asked if an 8dBm, 10MHz signal can be used as the single-ended CMOS input (REFA) for the AD9548. The final answer indicates that for VDD = 3.3V, the peak-to-peak voltage (1.58V) is less than the CMOS input high threshold (1.9V), so the signal cannot be reliably recognized. The user concluded that an additional amplification stage is required.
AI Generated Content

AD9548 的参考输入REFA 单端输入的功率大小?8dBm 的10MHZ 信号可以吗

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.