Post Go back to editing

AD9548 的参考输入REFA 单端输入的功率大小?8dBm 的10MHZ 信号可以吗

Thread Summary

The user asked if an 8dBm, 10MHz signal can be used as the single-ended CMOS input (REFA) for the AD9548. The final answer indicates that for VDD = 3.3V, the peak-to-peak voltage (1.58V) is less than the CMOS input high threshold (1.9V), so the signal cannot be reliably recognized. The user concluded that an additional amplification stage is required.
AI Generated Content

AD9548 的参考输入REFA 单端输入的功率大小?8dBm 的10MHZ 信号可以吗

Parents
  • 如下是 AD9548 单端 CMOS 输入的电气特性,根据供电电压不同,CMOS 输入逻辑阈值不同。

    假设 VDD = 3.3V,VIH = 1.9V,VIL = 1.0V,将 8dBm 转换为电压幅度(50Ω阻抗系统):

    Vrms≈0.56V  →  Vpp=1.58V<VIH=1.9V,无法保证 CMOS 输入被识别为逻辑高。

    在其他供电电压下的换算和比较方法与上述相同,供您参考。

Reply
  • 如下是 AD9548 单端 CMOS 输入的电气特性,根据供电电压不同,CMOS 输入逻辑阈值不同。

    假设 VDD = 3.3V,VIH = 1.9V,VIL = 1.0V,将 8dBm 转换为电压幅度(50Ω阻抗系统):

    Vrms≈0.56V  →  Vpp=1.58V<VIH=1.9V,无法保证 CMOS 输入被识别为逻辑高。

    在其他供电电压下的换算和比较方法与上述相同,供您参考。

Children