Post Go back to editing

ADF4368 使用EZSYNC同步问题

Category: Hardware
Product Number: ADF4368

各位专家,你们好,我最近的项目中用到了ADF4368,现在需要同步两片ADF4368。我采用了手册中推荐的EZSYNC同步的方法,通过各器件SPI产生同步脉冲,然后同时给各器件发送参考时钟来同步,以下是我的同步操作步骤和相关寄存器配置值:
1、0x2A地址bit 4写入0x0(目的是打开同步使能)
2、0x1F 地址bit 7写入0x0
3、0x1F 地址bit 7写入0x1
4、 0x1F 地址bit 7写入0x0(步骤2、3、4目的是通过SPI产生同步脉冲)
5、同时给两片ADF4368发送边沿对齐的参考时钟
6、0x2A 地址bit 4写入0x1(目的是关闭同步使能)
我按上述步骤执行后发现两片4368输出并未同步。我已经确认过输入参考时钟是完全对齐的,并且同时发送到两片4368,所以我想知道我的同步操作步骤是否正确,如果不对,正确的EZSYNC同步操作应该是怎样的,谢谢指导。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.