Post Go back to editing

AD9954可以设置成突发模式吗

Thread Summary

The user wants to configure AD9954 to output a 20 MHz sine wave burst for 100 clock cycles after a pin trigger. The final answer suggests using the single-burst mode to achieve this by providing 100 consecutive trigger signals. No other specific configuration details or alternative DDS chips were mentioned.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9954

想让AD9954输出一个突发波形,频率20M,通过一个引脚触发输出连续100个时钟周期的正弦波后就停止输出,如何设置呢,如果不能设置,有没有其他可以用的DDS芯片来实现这个功能呢,谢谢

I want AD9954 to output a burst waveform with a frequency of 20M. After triggering through a pin,it will output a sine wave for 100 consecutive clock cycles , then the output stop. How to set it? If it cannot be set, are there any other DDS chips that can be used to achieve this function? Thank you

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.