Post Go back to editing

issue that generate arbitrary waveforms

Thread Summary

The user inquires about generating 3 independent 100kHz arbitrary waveforms using the AD9106, which has 4 channels. The final answer confirms that this is possible, noting the device's on-chip pattern memory and DDS capabilities. The user should refer to the AD9106/AD9102 Low-Power DAC and Waveform Generator FAQs for configuration details, and ensure the SRAM data length corresponds to a full waveform cycle.
AI Generated Content
Category: Hardware
Product Number: AD9106

Hi ADI expert

    I am planning to generate 3 arbitrary signals of 100kHz. The AD9106 has 4 channels, can I generate 3 independent arbitrary waveforms of 100kHz.

    Thanks in advance!

Thread Notes