Post Go back to editing

AD9548寄存器配置与输出

Category: Software
Product Number: AD9548
Software Version: Linux

Hi:

1目的:我们板卡上AD9548输入SYSCLK频率125MHzREFAREFB均选择差分输入且优先级第1REFA(外部时钟源)、优先级第2REFB(本板时钟源,频率100MHz),期望OUT0~OUT3分别输出100MHz100MHz125MHz156.25MHz时钟。

2问题:现在调试期间使用ZYNQ7Z100在Linux下通过SPI接口配置AD9548REFA无输入时钟因此我们选择REFB100MHz时钟作为参考输入,现在我们对GUI使用不太熟悉,尝试很多次配置后DACOUP管脚虽然有时钟波形输出(非预期配置)通过外部模拟滤波后能够输入CLKIN,此后OUT0~OUT3无时钟信号输出。

3期望:希望能够提供技术支持指导我们使用GUI软件进行寄存器配置或者能够根据我们想要达到的目的提供一个Demo配置给我使用。

我的邮箱:luoxuwho@aliyun.com

谢谢!