Post Go back to editing

ADF4159 MUXOUT输出问题

Thread Summary

The user is experiencing issues with the N-Divider not detecting any signal in their custom PLL board, despite the R-Divider and N-Divider/2 working correctly. The PLL is not locking, and the VCO voltage is fluctuating between 1~1.8V. The support engineer suggests checking the oscilloscope settings, as the N-Divider output may have a very small duty cycle, and requests a screenshot of the oscilloscope measurement.
AI Generated Content

0x7

0x6

0x493335

0x84

0x1430003

0x42c800a

0x1

0x72ee0000

这是我的寄存器配置。寄存器写入顺序是R7~R0。 锁相环反馈的RFin是1.5Ghz,参考时钟REFin是50Mhz,R-DIVIDER可测到1Mhz的信号,N-DIVIDER/2可以测到500K的信号。

但是N-DIVIDER测不到任何信号这个不知道是为什么?

PLL目前也是一直未锁定,外接的VCO,测试cp输入VCO的电压是有的1~1.8V一直在波动

咨询一下各位,有遇到类似情况的吗?

  • Hi,

    Are you using an Evaluation board or a custom board? If you are using a custom board, did you simulate loop filter configuration with ADISimPLL? 

    The n-Divider output of the Mux will have a very small duty cycle. It is possible to miss pulses using an oscilloscope without the correct settings. A duty cycle of N-Divider output is heavily dependent on N divider value. The n-divider/2 output will have a 50% duty cycle because of dividing by 2. 

    Best Regards,
    Emrecan

  • 谢谢!!

    我使用的是自己做的板子,环路滤波器使用的是ADISimPLL计算的参数,环路滤波器参数应该没问题。

    我能确定N分频的数值是对的,对1.5Ghz分频1500得到的就应该是1Mhz的波形,N divider却测不到,N divider/2可以测到。N divider即使很小的占空比示波器也应该能测到吧?请问这可能是什么问题呢?

  • Hi,


    What are you seeing on an oscilloscope? is there any waveform?
    Can you take a screenshot from the oscilloscope while measuring the N-Divider output?

    Reards,
    Emrecan