Post Go back to editing

ADF4159 MUXOUT输出

Thread Summary

The user encountered an issue with the ADF4159 MUXOUT pin not outputting the expected 25 MHz in R-DIVIDER mode despite correct register settings. The problem was resolved by adjusting the write order of the registers, ensuring R0 is written last. The user also noted issues with N-DIVIDER mode, but this was not fully resolved in the thread.
AI Generated Content

有一个ADF4159 MUXOUT输出的问题想问一下大家。

我用的是50M的参考时钟,分频器型号为ADF4159CCPZ-RL7,VCO型号为HMC1167,寄存器从R7到R0分别设置的是

0x7
0x6
0x5
0x4
0x384C3
0x7108002
0x1
0x181CC000

想在MUXOUT引脚R-DIVIDER模式输出25Mhz的频率,但是不论怎么修改R0寄存器,R-DIVIDER模式出来的都是1.56Mhz,咨询一下各位如何解决

求教,感谢