Post Go back to editing

adf4159+hmc587实现扫频,滤波器设计问题

目标:扫宽5-8 GHz,周期600 μs的三角扫频

使用adf4159+hmc587,滤波器带宽1MHz,PFD频率100MHz

Q1.请问滤波器阶数应该选择三阶还是四阶呢?

Q2.图一是四阶的,C4=54.4 pF,VCO的输入电容是Ct=2.4pf,两者相差过大会有什么不好的影响吗?

 (图一)

Q3.图二是三阶的,我用的放大是OP184,Vr应该是多少呢?看到helpfile中Vr is set to 0.5*(Vmax + Vmin) where Vmax is voltage where the PD saturates when sourcing current,  and Vmin is the voltage where the PD saturates when sinking current.但我还是不太明白Vmax和Vmin代表什么。

 (图二)

Q4.另外,adf4159评估板的板载滤波器原理图中,OP184的+级还接了一些电阻和电容,而仿真设计的滤波器OP184+级是只接了偏置Vr,这里需要参考板载滤波器吗?

Q5.怎么确定滤波器的参数设置是否合理?

图三是采用三阶滤波器后的时域特性,是否输出正确的三角波,且满足所需的频率误差,滤波器设计就算完成,可以实际运用了?

 (图三)

感谢回复!