Post Go back to editing

Hmc701 register configuration

Thread Summary

The user is using HMC701 as a phase detector and HMC587 as a VCO to generate a 5-10 GHz output signal with a 100 MHz sine wave reference. The final answer confirms that this setup is feasible and suggests adjusting the HMC701's integer mode division registers to achieve the desired frequency range.
AI Generated Content

I use hmc701 as phase detector and hmc587 as VCO. I want to output 5-10ghz signal. The reference input of hmc701 is 100MHz sine wave. I use integer mode division to get a set of register parameters set to hmc701.

Parents Reply Children
No Data