Post Go back to editing

what's the Kv in ADIsimPLL software if the output volt from active filter is attenuated?

for example : Kv of RF wide band VCO is 200MHz/V。

normally, this Kv is final value. and the output signal from active loop filter goes to control VCO directly.

in my application, the output signal is attenuated, for exameple ,1/10.

then it goes to control VCO.

in this case . which one is right? 200MHz/V or 20MHz/V?

note: in ADIsimPLL software ,user need to input Kv of VCO.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.