Post Go back to editing

HMC4069一定要用推荐的有源环路吗?

Thread Summary

用户询问HMC4069有源环路滤波器设计问题,VCO调谐电压约为2.5V,但环路未锁定,调谐电压为4.8V。ADI支持工程师建议使用ADIsimPLL进行环路仿真,并确认HMC4069需要有源滤波。用户后来发现环路有时锁定,有时不锁定,最终更换HMC4069芯片解决了问题。
AI Generated Content

大家好:

我看HMC4069的数据手册中推荐了有源环路滤波器,但我实际用的VCO的tune电压约为2.5V。

1.现在按照数据手册有源电路设计的环路滤波器,放大器为ADA4625-1,其他值都和手册一样,HMC4069的参考为30.72MHz/sine/0dBm,VCO输入约为122.88MHz/sine/dBm,A0和A1为高测了约为3.1V(即4分频),供电5V/0.3A,但现在环路一直没有锁定,VCO的tune一直是4.8V,检查了好久没找到原因,请问有源环路输出2.5V是可以的吗?

2.可以用无源环路吗?只要满足手册NU,ND不小于2.5V?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.