English
EngineerZone
时钟与DDS
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
时钟与DDS
问答
文档
Members
Tags
Cancel
常见问题
马上提问
Open Questions. Can you
help
?
ADL5961上电120mA,后面按照上电顺序给电,下发命令没响应。设置IGAIN后回读寄存器为全0,帮忙看看是什么原因?
Not Answered
3 months ago
AD9528 同步脉冲请求问题
Not Answered
3 months ago
undefined
Not Answered
5 months ago
DDS AD9910
Not Answered
5 months ago
ad9528/ad9510测试板
Not Answered
5 months ago
该专区内容有关时钟与DDS的讨论和常见问题解答。 发帖前请阅读 Analog Devices EngineerZone 行为准则。
All Threads
by
HAHA123321HA
时钟与DDS
Latest
3 months ago
by
HAHA123321HA
348
2
0
Answered
多片AD9914同步问题
+1
Answered
现在我在使用三片AD9914进行SYNC_CLK的同步,我现在使用AD9513已经实现了三片SYNC_IN的同频同相,同时对三片芯片做了统一的DAC校准和IO_UPDATE,但是我没办法利用SYNCLK,因为他的驱动能力太弱了,现在的情况是我现在所做的步骤无法使我三片DDS的SYNC_CLK同步,请问可能是什么原因呢?如果我不拿SYNC_CLK做参考这个同步是可能的吗? REF_CLK是ADF4377提供的2.8GHZ提供给三片AD9914。
clock and timing
dds
Direct Digital Synthesis (DDS)
ad9914
348
2
0
by
HAHA123321HA
时钟与DDS
Latest
3 months ago
by
YANAMIANNA
276
1
0
Answered
AD9914上电波形小概率波形严重畸变
+1
Answered
AD9914使用DRG模式进行IOUPDATE触发式的生成脉冲内线性扫频信号,但是上电波形十次可能有一次波形严重不正常,如图和时频。
clock and timing
dds
Direct Digital Synthesis (DDS)
ad9914
276
1
0
by
JimHuang
时钟与DDS
Latest
3 months ago
by
JimHuang
225
2
0
Not Answered
ADL5961上电120mA,后面按照上电顺序给电,下发命令没响应。设置IGAIN后回读寄存器为全0,帮忙看看是什么原因?
0
Not Answered
ADL5961上电120mA,后面按照上电顺序给电,下发命令没响应。设置IGAIN后回读寄存器为全0,帮忙看看是什么原因?
225
2
0
by
wuwuwusan
时钟与DDS
Latest
3 months ago
by
Echen5
240
1
0
Not Answered
AD9528 同步脉冲请求问题
0
Not Answered
您好 我这里在配置9528时出现了一个问题 。 目前配置方式是通过SPI直接写寄存器地址来完成配置 出现这样一个问题 同步脉冲的触发方式目前为 SPI控制 我这里改写寄存器403的 bit0 是没有同步脉冲发出的?这是什么原因导致的? 测试环节: 1.在初始化配置是 直接将 BIT0 置1 无同步脉冲 2.先将所有寄存器进行配置(本次配置时bit0 为0)然后进行io更新。 更新后,重新配置寄存器403 (本次将bit0置1)然后再次寄存器更新 无同步脉冲
Clock Generation Devices
Clock Generation and Distribution
software
ad9528
240
1
0
by
Jesse__S
时钟与DDS
Latest
4 months ago
by
Jesse__S
306
2
0
Answered
使用AD9954/3/2/1的ASF调节输出波形幅值时,会影响DAC的输出位数吗?
+1
Answered
AD9954/ AD9953/AD9952/AD9951 有一个ASF(Amplitude scale factor)的14bit寄存器,可以调节输出波形的幅值,这里的幅值调节是否对AD9954内部14bitDAC的输出位数产生影响,是否还能保证在ASF修改为任意值时,DAC的输出位数都是14bit。如果修改ASF会影响DAC输出位数,那么有没有其他调节输出波形幅值的方法?
ad9954
Datasheet/Specs
clock and timing
dds
Direct Digital Synthesis (DDS)
Show More
306
2
0
by
SGSD
时钟与DDS
Latest
4 months ago
by
YANAMIANNA
216
1
1
Answered
AD9910
0
Answered
我设计的ad9910电路板,放在机箱中机箱模块5v供电,机箱收到静电时ad9910的输出会归零,通过spi读取寄存器,静电后cfr1,cfr2,cfr3这三个寄存器复位成默认值,其他step,range等寄存器保持不变。重新配置寄存器,ad9910输出恢复,我想知道静电影响了芯片的哪个位置或者引脚让cfr寄存器复位
hardware
clock and timing
Direct Digital Synthesis (DDS)
ad9910
216
1
1
by
DXXCCN
时钟与DDS
Started
5 months ago
130
0
0
Not Answered
undefined
0
Not Answered
你好,我使用AD9910进行多片同步,采用ADCLK854进行系统时钟分发差分晶振经过ADCLK854处理的时钟信号,同时采用ADCLK854进行同步的STNC-OUT信号的分发,时钟信号正常,SYNC-OUT输出正常,频率62.5MHz左右,但是接入主片,从片,一直显示无效电平状态,那个同步引脚一直为高,请帮忙提供下技术支持。
hardware
无效SYNC-IN信号
clock and timing
Clocks & Timers
dds
多片同步
Direct Digital Synthesis (DDS)
ad9910
Show More
130
0
0
by
DXXCCN
时钟与DDS
Started
5 months ago
112
0
0
Not Answered
DDS AD9910
0
Not Answered
你好,我使用AD9910进行多片同步,采用ADCLK854进行时钟分配,采用D触发器进行同步触发,系统采用40MHz晶振进行提供,通过分配器分发给9910,现在波形输出正常,有62.5MHz的同步信号输出,SYNC-CLK有250MHz的波形输出,但是一直显示未收到有效信号,同步引脚一直为高,请问我要怎么解决?
Datasheet/Specs
hardware
clock and timing
Clocks & Timers
Direct Digital Synthesis (DDS)
ad9910
Show More
112
0
0
by
QingGuang233
时钟与DDS
Latest
5 months ago
by
Echen5
272
1
0
Not Answered
ad9528/ad9510测试板
0
Not Answered
我需要对ad9528/ad9510进行初步测试,ad9528只需要测试其pll2和时钟分配功能,ad9510只需要测试其时钟分配功能,具体原理图如图 假设其余元件(有源晶振和电源)工作良好,这个测试板是否有致命缺陷?因为在尝试焊接后接电,ad9528出现明显发热到40+℃的情况,我想排除原理图问题
Clock Generation Devices
Clock Generation and Distribution
ad9528
ad9510
schematic
test borad
short circult
Show More
272
1
0
by
cp3kuo
时钟与DDS
Latest
5 months ago
by
Echen5
252
1
0
Answered
时钟管理芯片AD9517-4使用咨询
+1
Answered
请教AD9517-4使用问题: AD9517-4的out4~7即可以配置成lvds输出,也可以配置成cmos输出; 我在使用时,可以把out4与out5配置为lvd输出,另把out6与out7配置为cmos输出吗? 感谢~
Clock Generation and Distribution
252
1
0
View All Threads
by
HAHA123321HA
时钟与DDS
Latest
3 months ago
by
YANAMIANNA
276
1
0
Answered
AD9914上电波形小概率波形严重畸变
+1
Answered
AD9914使用DRG模式进行IOUPDATE触发式的生成脉冲内线性扫频信号,但是上电波形十次可能有一次波形严重不正常,如图和时频。
clock and timing
dds
Direct Digital Synthesis (DDS)
ad9914
276
1
0
by
HAHA123321HA
时钟与DDS
Latest
3 months ago
by
HAHA123321HA
348
2
0
Answered
多片AD9914同步问题
+1
Answered
现在我在使用三片AD9914进行SYNC_CLK的同步,我现在使用AD9513已经实现了三片SYNC_IN的同频同相,同时对三片芯片做了统一的DAC校准和IO_UPDATE,但是我没办法利用SYNCLK,因为他的驱动能力太弱了,现在的情况是我现在所做的步骤无法使我三片DDS的SYNC_CLK同步,请问可能是什么原因呢?如果我不拿SYNC_CLK做参考这个同步是可能的吗? REF_CLK是ADF4377提供的2.8GHZ提供给三片AD9914。
clock and timing
dds
Direct Digital Synthesis (DDS)
ad9914
348
2
0
by
Jesse__S
时钟与DDS
Latest
4 months ago
by
Jesse__S
306
2
0
Answered
使用AD9954/3/2/1的ASF调节输出波形幅值时,会影响DAC的输出位数吗?
+1
Answered
AD9954/ AD9953/AD9952/AD9951 有一个ASF(Amplitude scale factor)的14bit寄存器,可以调节输出波形的幅值,这里的幅值调节是否对AD9954内部14bitDAC的输出位数产生影响,是否还能保证在ASF修改为任意值时,DAC的输出位数都是14bit。如果修改ASF会影响DAC输出位数,那么有没有其他调节输出波形幅值的方法?
ad9954
Datasheet/Specs
clock and timing
dds
Direct Digital Synthesis (DDS)
Show More
306
2
0
by
SGSD
时钟与DDS
Latest
4 months ago
by
YANAMIANNA
216
1
1
Answered
AD9910
0
Answered
我设计的ad9910电路板,放在机箱中机箱模块5v供电,机箱收到静电时ad9910的输出会归零,通过spi读取寄存器,静电后cfr1,cfr2,cfr3这三个寄存器复位成默认值,其他step,range等寄存器保持不变。重新配置寄存器,ad9910输出恢复,我想知道静电影响了芯片的哪个位置或者引脚让cfr寄存器复位
hardware
clock and timing
Direct Digital Synthesis (DDS)
ad9910
216
1
1
by
oldeng
时钟与DDS
Latest
5 months ago
by
oldeng
303
1
0
Answered
ad9528 spi not respone
0
Answered
I have design a pcb use ad9528 to generate jesd204b clock for adrv9009. the schemtic is basiclly same as zcu102 and adrv9009 eval board. I try NO-OS sample of ADRV9009 .It exited at read device id . I have check the spi signal sended by xczu15eg...
Clock Generation Devices
Clock Generation and Distribution
hardware
ad9528
Wideband Transceiver IC
RF Integrated Transceivers
Show More
303
1
0
by
cp3kuo
时钟与DDS
Latest
5 months ago
by
Echen5
252
1
0
Answered
时钟管理芯片AD9517-4使用咨询
+1
Answered
请教AD9517-4使用问题: AD9517-4的out4~7即可以配置成lvds输出,也可以配置成cmos输出; 我在使用时,可以把out4与out5配置为lvd输出,另把out6与out7配置为cmos输出吗? 感谢~
Clock Generation and Distribution
252
1
0
by
Bing2510
时钟与DDS
Latest
6 months ago
by
Bing2510
289
2
0
Answered
AD9548 的参考输入REFA 单端输入的功率大小?8dBm 的10MHZ 信号可以吗
0
Answered
AD9548 的参考输入REFA 单端输入的功率大小?8dBm 的10MHZ 信号可以吗
Clock Generation and Distribution
Clock Synchronization
Clocks & Timers
289
2
0
by
QingGuang233
时钟与DDS
Latest
6 months ago
by
Echen5
236
1
0
Answered
AD9528 NVM
0
Answered
AD9528里有FLASH或者ROM能保存所有的寄存器设置吗?
Clock Generation Devices
Clock Generation and Distribution
flash
ad9528
nvm
rom
Show More
236
1
0
by
yyz1988
时钟与DDS
Latest
7 months ago
by
YANAMIANNA
290
1
1
Answered
AD9954可以设置成突发模式吗
0
Answered
想让AD9954输出一个突发波形,频率20M,通过一个引脚触发输出连续100个时钟周期的正弦波后就停止输出,如何设置呢,如果不能设置,有没有其他可以用的DDS芯片来实现这个功能呢,谢谢 I want AD9954 to output a burst waveform with a frequency of 20M. After triggering through a pin,it will output a sine wave for 100 consecutive clock cycles...
ad9954
Datasheet/Specs
clock and timing
Clocks & Timers
Direct Digital Synthesis (DDS)
Show More
290
1
1
by
chenfei123
时钟与DDS
Latest
7 months ago
by
Echen5
387
1
0
Answered
AD9912 输出杂散问题
0
Answered
我在使用AD9912时遇到输出杂散的问题:我给AD9912的输入参考时钟为1GHZ,器件disable时钟PLL功能,配置输出单频信号,例如手册中的201.1Mhz时从频谱仪上看500Khz窄带宽内杂散很少,并且幅度很小,SFDR能做到-90dbc。但是配置其它频点,例如200.001Mhz时,在500khz窄带宽内增加了很多杂散信号,SFDR只有-70dbc,这与手册中的指标相比差了很多,并且这些杂散均匀分布,各杂散频率间隔5khz,我不太清楚这是什么原因导致的。我试了很多输出频点,有一些频点信号窄带SFDR很好...
hardware
clock and timing
ad9912
Clocks & Timers
Direct Digital Synthesis (DDS)
杂散
Show More
387
1
0
View All Threads
更多内容
Post
Go back to editing
Filter
Show More