Post Go back to editing

《征文》+AD1955应用


 

ANALOG公司出品的高性能多位西格玛-德尔塔转换器件AD1955,该芯片为单电源供电,支持采样频率达192khz ,在48khz采样频率应用下信噪比可达120DB,内部整合有8倍过采样频率数字滤波器。方便设计者进行电路设计,并以较低的代价即可构成高性能的应用。在其他同类芯片中,还有CS4398PCM1798等也具有各自的特点,但是纵观ad1955的模拟转换器的电流输出能力,AD1955居然达到8.64ma P-P值,并且还需要设置有3.24ma的偏置输入电流保证,我们在实际应用往往容易发现一点,性能的提升必然要以功耗的付出做代价,效率的提升必然以工艺的改善为基础。

AD1955 DA转换器的内部功能块结构图如下图,从结构图就可以发现该芯片的应用设计极为简单明了,并无太多的逻辑设定。和CS8416一样,该芯片同样可以采用外部MCU控制使其工作于软件控制模式,但是该芯片的特点就是当没有外部MCU来写内部寄存器的时候,只要数据格式符合内部寄存器的初始默认值就可以正常工作,很方便设计者构成单片应用设计。对于AD1955的深层应用设计,在这里不再描述。

 

AD1955的引脚图如下图所示,对于不用的输入引脚(DSD数据输入端口),直接接地处理;不用的输出引脚(左右通道0标志输出引脚),悬浮处理;串行通讯口用上拉电阻接到电源即可。