Post Go back to editing

[征文]+[ 转载] 基于AD630锁相放大器的微弱信号检测(继两片AD9851使用心得后,再来一篇)

Thread Summary

The user discusses their experience with using the AD630 lock-in amplifier for weak signal detection, highlighting its ability to recover signals from 100 dB noise and its key features such as 2 MHz channel bandwidth, 45 V/μs slew rate, and -120 dB crosstalk at 1 kHz. The user emphasizes that the 9th pin should be connected to the carrier signal, not the modulated signal, to avoid incorrect output. The user also mentions challenges with phase differences in AM demodulation and suggests using a phase-locked loop (PLL) to overcome this issue.
AI Generated Content

[征文]+[ 转载] 基于AD630锁相放大器的微弱信号检测(继两片AD9851使用心得后,再来一篇)

去年8月参加了TI杯全国大学生电子竞赛,记得当初选题的时候,在A题微弱信号检测装置和B题频率补偿电路两题中徘徊,最好还是选择了B题频率补偿电路,获了个省三等奖TAT
    但是自己对微弱信号检测还是很感兴趣的,所以在比赛结束后,就自己把微弱信号检测做了一遍,开始时,选择使用取样积分来做微弱信号的提取,最后由于个人能力原因,未能成功,然后改为使用锁相放大来做,所以就选择了ADI公司生产的AD630。
    锁相放大器的原理我在此就不赘述了,大家有兴趣的可以去查看高普占写的《微弱信号检测》一书,里面对此已经进行了详细的介绍。
    锁相放大器中的相敏检测器是核心,相敏检测器鉴幅又鉴相,它的输出不但取决于输入信号的幅度,而且取决于输入信号与参考信号的相位差。常用的相位检测器有模拟乘法器MLT04和电子开关式AD630,实际上电子开关式相敏检测器相当于参考信号为方波的情况下的模拟乘法器。
   AD630电子式开关相敏检测器,AD630是一款高精度平衡调制器,采用灵活的换流结构,并由经过激光晶圆调整的薄膜电阻提供出色的精度和温度稳定性。其信号处理应用包括:平衡调制和解调、同步检波、相位检测、正交检波、相敏检测、锁定放大以及方波乘法。片上应用电阻网络提供±1和±2的精密闭环增益,精度为0.05% (AD630B)。这些电阻也可以用来精确配置多路复用器增益:+1、+2、+3或+4。或者,也可以采用外部反馈,允许设计人员实现高增益或复杂的开关反馈拓扑结构。AD630的功能框图如图1所示。
 
   AD630的特性有:

  可从100 dB噪声中恢复信号;

  频道带宽:2Mhz;

  压摆率:45V/us;

  串扰:-120 dB (1 kHz);

  引脚可编程、闭环增益:±1和±2;

  闭环增益精度和匹配:0.05%;

  通道失调电压:100 µV (AD630BD)

   350 kHz全功率带宽。
   AD630外接配置电路不同,实现的功能也不同,本次设计中使用AD630的锁定放大功能, 图1所示AMP A和AMP B分别配置为同相放大器和反相放大器,输入信号为待测信号和参考信号。待测信号同时输入到两个放大器中。参考信号输入到比较器中。待测信号在器件内部根据载波信号的正负进行翻转,实现了开关乘法功能。AD630的锁相放大电路示意图如图2所示。

   A点的波形为被检测信号与载波调制后的双边已调制波形,B点为双边已调制波形和噪声叠加后的波形,AD630的第9脚接载波信号,方波、正弦波都可行,相当与一个参考相位。AD630的输出接一个积分电路及一个低通滤波器,以达到的信号的完美恢复。
   AD630锁相放大的应用说明:
    锁相放大技术用于从干扰噪声中提取一个小并且带宽窄的信号,锁相放大器相当于一个检测器和一个窄带通滤波器的组合。当所需信号的频率和相位的是已知的情况下,非常小的信号可以从大量的不相关的噪声中检测出来。
   AD630组成的锁相放大器主要是由一个同步解调器组成,其次是一个低通滤波器。衡量锁相放大器性能的一个重要指标是其解调的范围。
   AD630的内部包含两个输入放大器,分别用于放大同相信号和反相信号;一个电子开关用作相敏解调,一个比较器用于将参考信号转换为方波信号,输出放大器兼有放大和低通滤波的作用。
   AD630的第13脚输出波形为一个含有载波的三角波,波形如图3所示,通过积分电路使其变为正弦波,再通过低通滤波器把载波滤除,就还原了噪声中的正弦波。

    值得注意的是,AD630作为锁相放大器时,第9脚为载波信号,并不是已调制信号,并且不能有直流偏置。如果将第9脚错误的接入了已调制信号,AD630将无法正确的输出,为杂乱的信号.
   对于AD630具体的参数以及相关说明,请参阅DATASHEET。以上只是我个人的看法~~~


Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.