Post Go back to editing

ADAS1000功耗与控制问题

1、参考ADAS1000的数据手册查找到高低性能模式下5输入通道+RLD等情况下的功耗数据,想问下该芯片上电后不做任何初始化设置大概消耗多大的电流(AVDD:3.3V,IOVDD:3.3V,内部供给DVDD&ADCVDD)?

2、ADAS1000的帧控制寄存器FRMCTL(0x0A)的[3:2]控制位控制跳过间隔,

00(默认值)= 每帧输出

01 = 每隔一帧输出

1× = 每隔3帧输出

[1:0]控制位设置:00,即2KHz的数据输出速率,如果我设置[3:2]位为01是不是数据输出速率为1KHz,设置为1x是不是数据输出速率为500Hz?

3、配置好ADAS1000后写帧表头寄存器FRAMES:0x40000000开始连续数据转换从SDO引脚输出,如果中途想停止ADAS1000的数据转换该如何停止?

谢谢!

Parents Reply Children
No Data