Post Go back to editing

AD7739  AINCOM端怎么接

请问AD7739输入差分应用时,AINCOM端怎么接?作为输入的参考端,一般应该接地,但数据手册中说明输入范围在0.2--AVDD-0.3,FIG27中用虚线连接参考电压正端。请专家指教

Parents
  • 实际使用时,采用单端输入,AINCOM端接到模拟地,也可以正确转换,是否可以这样使用?如果AINCOM端接到参考电压,是否意味着输入的小信号都是负值(只有输入大于参考电压的才为正值)?另外,用AD8253做正的直流毫伏信号放大时,有比较大的50Hz干扰,有好的推荐方法解决吗?当信号小(正值),放大倍数选择X1000时,会出现极性反转现象,输出很大的负电压,这是什么原因?AD8253后接AD7739(单端输入),AD8253的REF是否应该接AINCOM相同的电压?

Reply
  • 实际使用时,采用单端输入,AINCOM端接到模拟地,也可以正确转换,是否可以这样使用?如果AINCOM端接到参考电压,是否意味着输入的小信号都是负值(只有输入大于参考电压的才为正值)?另外,用AD8253做正的直流毫伏信号放大时,有比较大的50Hz干扰,有好的推荐方法解决吗?当信号小(正值),放大倍数选择X1000时,会出现极性反转现象,输出很大的负电压,这是什么原因?AD8253后接AD7739(单端输入),AD8253的REF是否应该接AINCOM相同的电压?

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.