Post Go back to editing

AD7739  AINCOM端怎么接

请问AD7739输入差分应用时,AINCOM端怎么接?作为输入的参考端,一般应该接地,但数据手册中说明输入范围在0.2--AVDD-0.3,FIG27中用虚线连接参考电压正端。请专家指教

Parents
  • AD7739可以采用单端输入也可以采用差分输入,AINCOM端是针对采用单端输入时的参考端,此时它的范围为0.2V到AVDD-0.3,FIG27中是采取单端输入的方式,虚线指的是这个AINCOM端可以接到参考电压或者外接一个在上述范围的电压值都可以;而如果采用的是差分输入,这个AINCOM端口可以悬空不接。

Reply
  • AD7739可以采用单端输入也可以采用差分输入,AINCOM端是针对采用单端输入时的参考端,此时它的范围为0.2V到AVDD-0.3,FIG27中是采取单端输入的方式,虚线指的是这个AINCOM端可以接到参考电压或者外接一个在上述范围的电压值都可以;而如果采用的是差分输入,这个AINCOM端口可以悬空不接。

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.