English
EngineerZone
线下专家面对面
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
线下专家面对面
Cancel
线下专家面对面
问答
讨论
文档
成员
标签
Cancel
Browse Our FAQs
Need Help? Ask a Question
This group hosts discussions and FAQs regarding 线下专家面对面. Please read the Analog Devices EngineerZone
Code of Conduct
before posting.
All Threads
by
ADIApproved
线下专家面对面
Latest
over 7 years ago
by
EZAdministrator
2324
1
0
Answered
ADI专家面对面之五——ADI产品介绍及其在各个领域中的应用
0
Answered
ADI 专家面对面是 ADI 公司与广大中小型客户以研讨会和客户拜访的形式直接交流的活动。 ADI技术专家现场指导客户如何应对实际设计应用中面临的问题,并详细讲解了用户在实际应用中遇到的常见问题和解决方法。 应广大客户的要求,我们将陆续上传 ADI 资深工程师们在研讨会现场的演讲 PPT ,以供大家参考,学习与探讨。 目前更新至第五场研讨会的内容。 第一场与第二场内容: 深度了解 16 位 8 通道同步采样数据采集系统 AD7606 第三场内容: 深入介绍放大器应用与经典案例分析...
2324
1
0
by
combrio
线下专家面对面
Latest
over 7 years ago
by
EZAdministrator
1123
1
0
Answered
AD7763 同步问题
0
Answered
按照datasheet中的要求,sync_n低电平最少2.5个ICLK周期,我将sync_n拉低了15个MCLK周期,MCLK频率为10MHz, ICLK频率为5MHz,相关信号时序波形如下所示,问题在于:sync_n拉高后,AD7763的fso_n信号一直为低,sdo信号一直为高,无法输出数据。注明:上图为下图中截取的一短时间内波形。
Single Channel A/D Converters
ad7763
Precision A/D Converters
1123
1
0
by
dataibao
线下专家面对面
Latest
over 7 years ago
by
EZAdministrator
1444
1
0
Answered
ADRF6602的寄存器中的值能读出来吗
0
Answered
您好: ADRF6602的寄存器中的值能读出来吗? 我的ADRF6602上电以后,DECL2P5引脚上可以量到2.5V的电压。DECL3P3引脚上有时可以量到3.3V的电压,有时只有500mv的电压。VTUNE引脚上有时可以量到1.78V的电压,有时只有50mv的电压。DECLVCO有时可以量到2.89V的电压,有时只有50mv的电压。我看资料0x06寄存器可以控制3.3V LDO。于是我主程序就写了一个循环 while(1) { ADRF6602_reg_write(LDO_3V3_ENABLE...
寄存器读写
1444
1
0
by
王林申
线下专家面对面
Latest
over 7 years ago
by
EZAdministrator
1397
2
0
Answered
全桥控制
0
Answered
请问ADI有全桥开关电源控制IC吗?有的话是什么型号?
1397
2
0
by
xiongyd
线下专家面对面
Latest
over 7 years ago
by
EZAdministrator
1291
2
0
Answered
AD5737上电后芯片过热
0
Answered
您好,用到贵公司的AD5737芯片,芯片上电后会发热的比较厉害,用SPI读取寄存器,SDO总线也没有接到任何数据,SPI的SDI总线的数据均符合AD5737上面的时序,目前不知道问题出在哪里,附上原理图,希望您能够看看是否有错误的地方,万急!!! 其中 电感没有10uh的 目前用1uh的在调试,其他的均和原理图一样。问题找了好久都没有结果,希望能够尽快恢复!!谢谢!!不胜感激!!
4-20mA Current Loop D/A Converters
ad5737
Precision D/A Converters
1291
2
0
by
fugui_jiang
线下专家面对面
Latest
over 7 years ago
by
EZAdministrator
1300
2
0
Answered
ADAS1000功耗与控制问题
0
Answered
1、参考ADAS1000的数据手册查找到高低性能模式下5输入通道+RLD等情况下的功耗数据,想问下该芯片上电后不做任何初始化设置大概消耗多大的电流(AVDD:3.3V,IOVDD:3.3V,内部供给DVDD&ADCVDD)? 2、ADAS1000的帧控制寄存器FRMCTL(0x0A)的[3:2]控制位控制跳过间隔, 00(默认值)= 每帧输出 01 = 每隔一帧输出 1× = 每隔3帧输出 [1:0]控制位设置:00,即2KHz的数据输出速率,如果我设置[3:2]位为01是不是数据输出速率为1KHz...
Biopotential Sensors
adas1000
Bio-Sensors
1300
2
0
by
dataibao
线下专家面对面
Latest
over 7 years ago
by
EZAdministrator
2197
2
0
Answered
关于ADL5501外围电路的疑问
0
Answered
您好: 我查阅资料,看到ADL5501的第二个管脚FLTR(Square-Domain Filter Pin)要外接一个电容并接高电平,在焊接的时候可以不焊。我的项目对空间要求较高,我在电路中没有设计这个外接电容,但是我担心不接这个电容会影响我输出电压和输入电压有效值之间的线性度关系。 问题1:请问不接这个电容CFLTR是否会影响ADL5501的线性度?这个电容具体会影响哪些指标?什么时候应该接,什么时候可以不接? 另外,ADL5501的第六个管脚VRMS除了接滤波电容COUT外还接了一个电阻ROUT...
adl5501
RMS Detectors
RF Power Detectors
2197
2
0
by
EEG
线下专家面对面
Latest
over 7 years ago
by
EZAdministrator
1486
3
1
Answered
多通道放大器共模抑制比下降
0
Answered
在设计40导EEG放大器时,前级使用AD620,将40个AD620负端接参考REF电极时,每通道CMRR会下降,请问措施?
amplifiers
eeg
Instrumentation Amplifiers
ad620
1486
3
1
by
harry.wei
线下专家面对面
Latest
over 9 years ago
by
sulje
1079
1
0
Discussion
如何利用Visual DSP++或CCES调试Blackfin ldr程序
Discussion
在使用 Blackfin 开发产品时也许你会遇到这样的问题:在 VDSP或者CCES 下调试 dxe ,一切都正常,但是烧写 ldr 脱机运行时,程序甚至连启动都不能启动。附件分别以 BF518 和 BF609 为例,简单介绍了调试 ldr 的方法。
cces
boot
visualdsp
ldr
blackfin
Show More
1079
1
0
by
viicauss
线下专家面对面
Latest
over 9 years ago
by
lizhuo
4147
10
0
Answered
AD9361 能实现零中频吗?
0
Answered
您好,请问射频信号通过AD9361 能下变频到基带信号吗,能实现零中频吗?
ad936x
ad9361
sdr
Wideband Transceiver IC
RF Integrated Transceivers
Show More
4147
10
0
View All Threads
by
zhangsx1289
线下专家面对面
Latest
over 11 years ago
by
ADIApproved
1211
1
0
Answered
关于频率变化的正弦波幅值信息提取
0
Answered
有一个近似正弦波的信号,信号频率从 10MHz 到 40MHz 变化,信号的幅值也在变化,变化的幅度在 200mV 到 800mV 之间。现在想把这个信号的幅值信息提取出来,提取出来的信号与其频率无关。希望得到的这个信号,其幅度随着原来正弦波幅值的变化而变化。 大家有什么好的想法吗?
正弦波幅值
1211
1
0
by
guoshenghe
线下专家面对面
Latest
over 11 years ago
by
ADIApproved
1222
2
0
Answered
ad9364 多载波设置
0
Answered
请问怎样可以生成一个 带宽为4MHz (OFDM qpsk)+280KHz(BPSK)信号,用于9364发射,总的带宽不超过5MHz,280KHz的信号可以偏离4M信号带外最大1MHz?
sdr
Wideband Transceiver IC
ad9364
RF Integrated Transceivers
ad9364 多载波设置及生成
Show More
1222
2
0
by
ppa3278
线下专家面对面
Latest
over 11 years ago
by
▓巭孬▓
879
1
0
Answered
我想得到一个0.2毫伏VPP,频率150KHz的正弦波,有什么好办法?
0
Answered
由于我使用的信号源分辨率16位,达不到这个要求,衰减设计起来也麻烦,信号源内阻,负载的阻抗都不确定。。有什么好的芯片能实现吗?
信号源分辨率
879
1
0
by
杨先生
线下专家面对面
Latest
over 11 years ago
by
adi_rock
952
1
0
Answered
如何读取评估板adisusbz数据
0
Answered
手上有一个adis16405的IMU,和一个评估板ADISUSBZ。通过测试软件已经确认设备完好。 现在希望通过labwindows/cvi编写一个程序,通过USB口直接读取到传感器的数据,不知道有没有高人给指点一下该怎么办,或者有相关可以参考的文件例程可以联系我。 yang_yunkai@yahoo.com 在下感激不尽。
sensors
Inertial Measurement Units (IMU)
Sensors and MEMS
adis16405
adisusbz
Show More
952
1
0
by
何镇江
线下专家面对面
Latest
over 12 years ago
by
ADI_Eva
1565
2
0
Answered
关于使用ADV212 压缩解压1080p 30帧 的 大概处理过程,关于ADV212没有提供标准编解码,只有自己配置,我想知道具体配置是怎么回事?谢谢回答。
+1
Answered
使用两片ADV212编解码 1080p 30帧图像 寄存器配置问题
Video Products
adv212
30
video compression
1080p
Show More
1565
2
0
by
hu3692@163.com
线下专家面对面
Latest
over 12 years ago
by
ADIApproved
2393
5
0
Answered
BBPLL_REF_CLK时钟未锁定,但是有频率,是怎么回事?
0
Answered
你好,我在进行AD9361的配置上面出现了如下的问题: 1. Calibration TIMEOUT (0x5E, 0x80) clk_set_rate,source:3,phy->clks[source]->rate:983040000 //3为 BBPLL_REF_CLK 我的分析:从Calibration TIMEOUT 上看是因为时钟没有锁定,但是后面后面可以看见时钟其实已经起来了,我想问的是,这个时钟是不是我配置的时钟还是我输入进去的时钟?因为 AD9361_InitParam...
ad9361
Wideband Transceiver IC
RF Integrated Transceivers
2393
5
0
by
houwenhe
线下专家面对面
Latest
over 12 years ago
by
adi_rock
1610
2
0
Answered
关于ADXL278 SELF TEST的使用问题
0
Answered
最近要用到ADI的ADXL278 这款高g的加速度计,现在遇到一个问题就是:self test 如何使用,通篇 阅读datasheet也没有具体使用细节,只是介绍了基本校准原理,输入电压范围。具体怎么使用呢,输入怎么才能激活,什么样的信号才能激活自测?需不需要读输出?有没有介绍self test的文章?希望得到高手解答,谢谢!
self
sensors
accelerometers
Sensors and MEMS
test
adxl278
Show More
1610
2
0
by
江南四月
线下专家面对面
Latest
over 12 years ago
by
adi_rock
1310
2
0
Answered
AD9215内部参考电压不正确
0
Answered
最近做了一块PCB,上面的AD9215使用内部参考电压,正常应该是1V。但是有一块板子的AD9215出问题了,刚上电时参考电压120mv,逐渐增大,最后稳定在电源电压3.3V附近。这导致刚上电AD9215不工作。请问这是什么原因?是片子坏了吗?
ad9215
High Speed A/D Converters >10 MSPS
Standard High Speed A/D Converters
1310
2
0
by
zpy
线下专家面对面
Latest
over 12 years ago
by
adi_apple
2926
5
0
Answered
AD7739 AINCOM端怎么接
0
Answered
请问AD7739 输入差分应用时,AINCOM端怎么接?作为输入的参考端,一般应该接地,但数据手册中说明输入范围在0.2--AVDD-0.3,FIG27中用虚线连接参考电压正端。请专家指教
Multiplexed A/D Converters
ad7739
Precision A/D Converters
2926
5
0
by
hansir
线下专家面对面
Latest
over 12 years ago
by
frank.wu@analog.com
2016
3
0
Answered
请问在官网下载的原理图(不是PDF文件)用什么软件打开?
0
Answered
在官网上下了TS201开发板的原理图,其中有开发的原理图封装等压缩包文件,后缀名为*.1、*.2、*.3...等这种的文件,应该是代表着原理图的第1、2、3....层,说明文档上标明该原理图是使用DxDesigner 2007画的,但是其中只有一个.asc文件,不知道用什么软件可以打开这些原理图文件呢?
ts201开发板
2016
3
0
View All Threads
更多内容
Post
Go back to editing
Filter
Show More