hello ,I find in the enginerrzone,there is a link : Problem with setting AD9361 bandwidth using libiio
why tx and rx bandwidth is not the same as 56M?
2\and I want to know whether mimo 2*2 RX or TX max bandwidth change or not?
thanks.
hello ,I find in the enginerrzone,there is a link : Problem with setting AD9361 bandwidth using libiio
why tx and rx bandwidth is not the same as 56M?
2\and I want to know whether mimo 2*2 RX or TX max bandwidth change or not?
thanks.
add description:
I find a tab from a document <AD9361_Reference_Manual_UG-570.pdf> , I'm confused. Why is 1T1R twice as fast as 2T2R(max data rate (combined I and Q words))???
At UG-570 page 92, just above the Table 48, write:"The maximum DATA_CLK rate is limited to 61.44 MHz, so the data rates are limited by this factor and the 56 MHz maximum analog filter bandwidth". So at CMOS interface, the data rate is limited by DATA_CLK rate