二块AD9370板(采用的是artix7 fpga),两块板稍微有一点不同,都是AD9528和AD9370的SPI由stm32芯片控制,其中一块板(称为A板) AD9528和AD9370的spi都正常了,fpga要用的频率也由ad9528产生了,AD9370的0x03和0x20寄存器实验测试也正常,但另一块板B的ad9528频率正常,且fpga闪灯实验正常,给ad9370的电源和复位信号都是正常的(和A板一样的操作),但RBIAS脚却没有0.7V左右的电压,所以ad9370的spi口读0x03寄存器返回值不是9而是FF,请问,我还要如何查找问题或如何解决问题?