Post Go back to editing

ad9375输出信号功率偏小问题

您好!我使用的是zcu102+ad9375,在fpga中,我使用的是xilinx jesd204b的ip核,如果将ip核配置为N=14(实际ip核配置需减1),CS=2,基带信号使用14bit位宽的dds产生,在vhdl文件中:

assign lane0 <= {s1[7:0],2'b0,s1[13:8],s0[7:0],2'b0,s0[13:8]};

输出频谱正确,但功率只有-12dbm,如果开启ad9375内部nco,输出功率有0dbm。

如果将ip核配置为N=16(实际ip核配置需减1),CS=0,基带信号使用16bit位宽的dds产生,在vhdl文件中:

assign lane0 <= {s1[7:0],s1[15:8],s0[7:0],s0[15:8]};

输出频谱不正确,可以看出,实际ad9375使用的是低14bit,这与ug-992的描述不符。

我尝试修改ad9375中deframe的配置,无论怎么修改N与CS,始终发送低14bit数据频谱正确,且只有-12dbm,高14bit频谱不对。

我怎么才能提高输出功率?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.