Post Go back to editing

3 導程(Lead I, Lead II, Lead III)量測

Thread Summary

用户询问MAX30001是否可以用于三导联(Lead I, Lead II, Lead III)测量。最终答案指出MAX30001内部只有一个ECG通道,因此无法实现三导联测量。建议使用ADAS1000作为替代方案。
AI Generated Content
Category: Hardware
Product Number: MAX30001

MAX30001可以用來做3導程(Lead I, Lead II, Lead III)量測嗎?    如果可以,需要如何設計?

或者有其他推薦元件可以用來做3導程的量測?