Post Go back to editing

MAX30009上位机是如何换算阻抗值?

Thread Summary

用户在使用MAX30009评估板进行4线法阻抗测量时遇到计算出的阻抗模值不准确的问题。最终答案建议用户按照附件中的方法对纯电阻进行测量,并使用提供的计算表导出测量结果以立即获得误差分析。校准参数应参考数据手册和附件。
AI Generated Content

各位好,

    最近我在使用max30009的评估板进行4线法阻抗测量测试时,发现参考应用手册的标定方法无法计算出有效的阻抗模值,但是上位机显示是正确的。

但是,我将测试的数据导出来之后,参考手册的计算方式进行计算;使用1K的电阻进行外部校准,校准参数如下图所示

计算出来的阻抗模值并不是510Ω,而是77100这样的数据,请问这是什么原因导致的?

Parents Reply Children
No Data