Post Go back to editing

AD5941与nrf52832的数据传输问题

Thread Summary

The user encountered an issue where the nRF52832 reads the same constant value from the AD5941 when using the Ramp example code, despite successfully reading the device ID with the SPI example. The final answer indicates that the issue will be further discussed via email. The AD5941 and nRF52832 are the key components involved.
AI Generated Content
Category: Software
Product Number: AD5941

使用AD5941自带的Ramp例程采集数据,随后将采集到的数据通过SPI通信传输给nrf52832。我们根据官方提供的代码移植方式进行了移植,使用提供的SPI例程可以成功读取到器件ID,但使用Ramp例程后nrf52832从SPI读取的数据一直是同一个不变的值。我想知道问题大概出现的哪里?有什么方式可以快速的排查出问题在哪?SPI_RAMP.rar

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.