Post Go back to editing

ADAS1000,如果人体阻抗过大,导联脱落后无法检测到再连接

Thread Summary

用户在使用ADAS1000时发现,当人体阻抗为16MΩ且RA导联电压抬升到5V左右时,导联脱落后无法重新检测到连接。最终答案建议如果是交流导联脱落检测,增加阈值电压;如果是直流导联脱落检测,减小增益。在12导模式下,用户需要配置相关寄存器来减小增益。
AI Generated Content
Category: Hardware
Product Number: ADAS1000

现象:实测发现ADAS1000,如果连接人体,人体毛发较多的时候,第一次能连接成功,但是脱落后无法再检测到连接的问题.

实测:

         1、人体阻抗用电阻模拟16MΩ,导联脱落后,RA导联电压抬升,如果抬升到4V以内的时候,物理导联再次连接,ADAS1000能检测到连接,否则无法检测到连接。

         2、人体阻抗用电阻模拟4MΩ,导联脱落后,无论什么时候物理导联再次连接,ADAS1000都能检测到连接。

问:人体阻抗用电阻模拟16MΩ,请问当RA导联电压抬升到5V左右时,如果通过配置寄存器的方式,让导联脱落和连接检测恢复正常?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.