Post Go back to editing

AD5933写入与读取失效问题

Thread Summary

用户在使用AD5933时遇到读取Status和Data寄存器数据无变化的问题,尤其是在设备持续运行后。最终答案指出问题可能源于程序编写不正确,特别是DFT输出处理不当。建议参考相关帖子和AD5933例程进行程序修正。
AI Generated Content
Category: Hardware
Product Number: AD5933

您好!我在应用AD5933时出现一个无法解决的问题,详情如下:在设备持续读取一段时间的数据之后,偶发性地出现读取Status和Data寄存器数据无变化的问题。此时尝试使用reset或powerdown指令复位AD5933后读取状态寄存器值仍不变(固定为0x56),使用示波器观察I2C信号读写正常。请问AD5933内部是否有锁存操作或其他任何可能因素导致这种情况发生?非常着急,请尽快回复,万分感激!

Thread Notes

Parents Reply Children
No Data