ADUCM355使用M355_ECSns_EIS程序进行EIS扫频1K电阻,在低频率时阻抗值和相位值都出现了异常
问答
讨论
文档
Members
Tags
Cancel
Thread Details
State
Verified Answer
Replies
4 replies
Subscribers
2 subscribers
Views
718 views
Users
0 members are here
Options
Share
More
Cancel
Related
Post
Go back to editing
ADUCM355使用M355_ECSns_EIS程序进行EIS扫频1K电阻,在低频率时阻抗值和相位值都出现了异常
LCHuang
on Aug 6, 2025
Thread Summary
用户在70Hz之前的频率测试中遇到电阻值异常的问题,70Hz及以上的频率测试结果正常。Analog Devices支持工程师建议检查板上的校准电阻RCAL值是否与程序中的值一致,并且与实际被测电池内阻值差距不大。用户确认RCAL值为200Ω,但在低频测试时仍存在较大偏差。
AI Generated Content
在70Hz之前的电阻值都出现异常,在70Hz之后的才正常
不正常的数据如下
正常的数据如下
sensors
Sensors and MEMS
aducm355
eis
Electrochemical Sensors