Post Go back to editing

MAX31856测试温度的稳定有效值位数

Thread Summary

用户询问MAX31856测试温度时的稳定有效值位数,实际测试中温度读数在0.1℃范围内跳变。支持工程师解释说,由于冷端温度准确性和热端温度准确性的限制,0.1℃的跳变是正常的。用户确认芯片手册上温度数据分辨率为0.0078125℃,但实际稳定度只能达到0.1℃,并接受了这一现象是芯片特性决定的。
AI Generated Content
Category: Hardware
Product Number: MAX31856, MAX3185

 您好!MAX31856测试温度时的稳定有效值位数是几位?我的实际测试稳定读数是0.1℃的跳变,0.1℃以后的读数跳变很大,不知道这种现象是不是正常?

Thread Notes

Parents
  • 对于MAX31856,其本身温度精度受到两个因素影响:

    1、冷端温度准确性:±0.7°C (max, -20°C to +85°C)

    2、热端温度准确性:±0.15% (max, -20°C to +85°C)

    因此,综合以上两组数据,0.1℃的跳变是可以接受的。

  • 非常感谢您的回复!因为是首次使用MAX31856芯片,对该芯片的特性不熟悉,从芯片手册的数据上获悉该芯片的温度数据分辨率为0.0078125°C,预期的数据稳定度在0.01°C,但是,实际板子的测试温度值的稳定读数在0.1°C上下跳变,如果保留2位小数,采样的温度值在0.02到0.06跳变,所以第二位小数值跳变很大,只能保留一位小数,数据看起来比较温度。为了排除是板子布线和电源其他问题,所以想请教一下有经验的大佬给答疑一下,看了您的回复,我可以排除是其他问题了,这个芯片的特性决定了,稳定度就是这样

Reply
  • 非常感谢您的回复!因为是首次使用MAX31856芯片,对该芯片的特性不熟悉,从芯片手册的数据上获悉该芯片的温度数据分辨率为0.0078125°C,预期的数据稳定度在0.01°C,但是,实际板子的测试温度值的稳定读数在0.1°C上下跳变,如果保留2位小数,采样的温度值在0.02到0.06跳变,所以第二位小数值跳变很大,只能保留一位小数,数据看起来比较温度。为了排除是板子布线和电源其他问题,所以想请教一下有经验的大佬给答疑一下,看了您的回复,我可以排除是其他问题了,这个芯片的特性决定了,稳定度就是这样

Children
No Data