Category: Hardware
Product Number: MAX31856, MAX3185
您好!MAX31856测试温度时的稳定有效值位数是几位?我的实际测试稳定读数是0.1℃的跳变,0.1℃以后的读数跳变很大,不知道这种现象是不是正常?
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 0 hours |
ADIYX |
Open |
您好!MAX31856测试温度时的稳定有效值位数是几位?我的实际测试稳定读数是0.1℃的跳变,0.1℃以后的读数跳变很大,不知道这种现象是不是正常?
ADIYX - Moved from 接口和隔离专区 to 生物/电化学/磁场/温度传感器专区. Post date updated from Sunday, June 29, 2025 11:22 AM UTC to Friday, July 4, 2025 2:13 AM UTC to reflect the move.
对于MAX31856,其本身温度精度受到两个因素影响:
1、冷端温度准确性:±0.7°C (max, -20°C to +85°C)
2、热端温度准确性:±0.15% (max, -20°C to +85°C)
因此,综合以上两组数据,0.1℃的跳变是可以接受的。
非常感谢您的回复!因为是首次使用MAX31856芯片,对该芯片的特性不熟悉,从芯片手册的数据上获悉该芯片的温度数据分辨率为0.0078125°C,预期的数据稳定度在0.01°C,但是,实际板子的测试温度值的稳定读数在0.1°C上下跳变,如果保留2位小数,采样的温度值在0.02到0.06跳变,所以第二位小数值跳变很大,只能保留一位小数,数据看起来比较温度。为了排除是板子布线和电源其他问题,所以想请教一下有经验的大佬给答疑一下,看了您的回复,我可以排除是其他问题了,这个芯片的特性决定了,稳定度就是这样