Category: Hardware
Product Number: AD5941
想做一个测量金属/涂层的阻抗测量电路。阻抗测量范围1kΩ~10MΩ。频率测量范围:1Hz~10kHz。
看了一下材料,AD5933很常用,好像测量1Hz低频时有困难?AD5941合适吗?能推荐几款合适的芯片供选择吗?非常感谢!
想做一个测量金属/涂层的阻抗测量电路。阻抗测量范围1kΩ~10MΩ。频率测量范围:1Hz~10kHz。
看了一下材料,AD5933很常用,好像测量1Hz低频时有困难?AD5941合适吗?能推荐几款合适的芯片供选择吗?非常感谢!
Jackie Wang - Moved from MEMS专区 to 生物/电化学/磁场/温度传感器专区. Post date updated from Saturday, September 28, 2024 2:21 PM UTC to Tuesday, October 8, 2024 6:42 AM UTC to reflect the move.
AD5940/1频率范围是0.015Hz~200kHz,应该是符合要求的。
谢谢。5940的阻抗测量范围官方手册没写,查了一些资料,好像大阻抗(比如超过1M)时精度较低。