Category: Datasheet/Specs
Product Number: AD5940
我们想用AD5940做八电极的体脂秤,但是官方的应用文档只有 2线生物阻抗和 4线BIA两个例子。请问AD5940能做八电极的BIA吗?
我们想用AD5940做八电极的体脂秤,但是官方的应用文档只有 2线生物阻抗和 4线BIA两个例子。请问AD5940能做八电极的BIA吗?
Jackie Wang - Moved from 精密转换器专区 to 生物/电化学/磁场/温度传感器专区. Post date updated from Wednesday, September 11, 2024 8:35 AM UTC to Thursday, September 12, 2024 2:50 AM UTC to reflect the move.
AD5940/1里面的ADC只有一个,因此最多转换一个响应信号,最多支持4电极
4线BIA中使用CE0--AIN2--AIN3--AIN1,可以通过开关矩阵切换到其他IO脚吗?我们每次只会用4线,但是希望使用8个IO脚,根据需要每次选4个IO脚来测量阻抗,这样来测量身体不同部位,请问AD5940可以实现吗?
建议外加多路选择开关mux实现
外加多路选择开关mux实现的方法,你们有实际应用过吗?也就是我想知道这个方法是否切实可行。另外,我们使用其它芯片方案,多次测量阻抗会出现波动比较大情况,请问AD5940有没有重复性测试的相关数据?
外加多路选择开关mux实现的方法,你们有实际应用过吗?也就是我想知道这个方法是否切实可行。另外,我们使用其它芯片方案,多次测量阻抗会出现波动比较大情况,请问AD5940有没有重复性测试的相关数据?
有其他客户正在评估多路开关+AD5940的方案,但是具体效果如何尚未知晓。IC在设计和生产过程中需要经过多次测试,您可以采取AD5940的评估板对纯电阻进行测试,看看重复性是否能获得您的满意。如您确实担心多路开关的影响,可以采用两片AD5940并联。