Post Go back to editing

ADAS1000主从机配置实现12导联

Category: Hardware
Product Number: ADAS1000


我使用两个ADAS1000,配置成主从机模式,实现12导联系统,其他配置正确,有数据输出,关于输出的数据格式,有以下疑问:
我想要直接读取到12个导联的数据,按照手册说的将主器件配置为导联模式,从器件配置为电级模式,这样别从主器件和从器件上获取到的数据即为对应的9导联数据,主机上的数据对应LEAD_I、LEAD_II、LEAD_III、LEAD_V1、LED_V2,从机数据对应LEAD_V3、LEAD_V4、LEAD_V5、LEAD_V6,另外3个扩展导联数据自己通过以获取的导联数据计算获得不知道我这样理解是否正确,不正确的话麻烦大家指导一下正确的配置方式

Thread Notes

Parents
  • 作为电极模式的芯片输出的是电极电势,作为导联模式输出的才是算好的心电电压(也就是电极电势差)。需要将从机ADAS1000的输出(V3~V6的电势)减去根据主机ADASD1000的输出(通过I/II/III)计算而得到的WCT,从而得出V3~V6的导联电压。这一步骤需要在MCU上面实现。

Reply
  • 作为电极模式的芯片输出的是电极电势,作为导联模式输出的才是算好的心电电压(也就是电极电势差)。需要将从机ADAS1000的输出(V3~V6的电势)减去根据主机ADASD1000的输出(通过I/II/III)计算而得到的WCT,从而得出V3~V6的导联电压。这一步骤需要在MCU上面实现。

Children