Post Go back to editing

maxm86161

Category: Software
Product Number: maxm86161

我们使用MAXM86161的时候遇到了一个问题,我们的IIC总线上挂载了三个芯片,目前只有MAXM86161无法通信,IIC总线速率为100K,EN引脚测试为3.3V,芯片供电测试为3.3V,IIC总线上发送指令后设备未响应,能帮忙排查一下问题吗?

Thread Notes

  • 1、VREF是否量取到1.21V左右的电压?如果没有此电压输出IC是工作不正常的。

    2、是在什么渠道购买的IC?

  • MCU的IO口的初始化问题。请问一下,MAXM86161的低功耗模式的工作电流大概是多少?我这边测试,只要外部en引脚使能,打开这个芯片的功耗有700uA,哪怕设置shutdown模式依然有400uA功耗,这个是什么原因帮忙看一下,谢谢!

  • 问题描述:
    设备在待机时会拉低LDO_EN,在采样开始时拉高LDO_EN,但是LDO_EN一旦拉高就有700ua的大电流,此时我们的传感器配置为14.8us,16kADC,24sps,三个LED通道电流分别是0x0d,0x0a,0x14,其他功能全部关闭

    问题跟进:
    1. 我们将LED灯完全关闭,电流变为400ua,此时传感器配置为14.8us,4kADC,24sps,其他功能全部关闭

    问题影响:
    这个功耗在我们的产品上完全无法使用,我们期望和手册中描述的Low-Power Operation, Optical Readout Channel <
    10μA, Typical at 25sps 这条信息一样的功耗标准,我们能接受LED灯存在功耗,但不能接受采集通道如此之高

  • 您好,目前此问题已经解决,在上电初始化复位时,设置如下0x00和0x01寄存器后功耗测试正常。
    代码如下:
    READ Interrupt_Status_1; // Clear Interrupt (Register 0x00)
    READ Interrupt_Status_2; // Clear Interrupt (Register 0x01)

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.